DOCA0161ENUS-01

Contactor utilization categories (IEC 60947-4-1)

The standard defines four utilization categories, AC1, AC2, AC3 and AC4 depending on the load and the control functions provided by the contactor. The class depends on the current, voltage and power factor, as well as contactor withstand capacity in terms of frequency of operation and endurance.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.