DOCA0161ENUS-01

SDTAM thermal fault module

Relay module with two static outputs specifically for the motor-protection Micrologic 2 M trip units. An output, linked to the contactor coil, opens the contactor when an overload or other motor fault is detected, thus avoiding opening of the circuit breaker. The other output stores the opening event in memory.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.