DOCA0161ENUS-01

Isd: Short-time protection with fixed time delay

This protection supplements thermal protection. Short-time protection, but with a fixed time delay. This function is available on Micrologic 2M. The short-time pick-up Isd is adjustable from approximately 5 to 13 Ir.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.