DOCA0161ENUS-01

Iunbal: Phase-unbalance or phase-loss protection

This protection function steps in if the current values and/or the unbalance in the three phases supplying the motor exceeds tolerances. Currents should be equal and displacement should be one third of a period. Phase-loss is a special case of phase-unbalance.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.