JYT97577–01

Circuit Breaker Communication Module (BSM or BSCM)

A module which, when installed in a circuit breaker, receives and transmits information on the communication network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.