JYT97577–01

I-Line Enable Module Installation

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm that all power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • Qualified persons performing diagnostics or troubleshooting that require electrical conductors to be energized must comply with NFPA 70 E—Standard for Electrical Safety Requirements for Employee Workplaces and OSHA Standards—29 CFR Part 1910 Subpart S—Electrical.
Failure to follow these instructions will result in death or serious injury.

NOTICE
HAZARD OF equipment damage
  • Do not adjust jaws.
  • Do not remove joint compound.
  • If necessary, use Square D joint compound PJC7201.
Failure to follow these instructions can result in equipment damage.

I-Line Enable Module Installation Instructions

Follow this procedure to install the I-Line Enable Module. Refer to the Figures at the end of this section to assist with the installation instructions:
  1. Turn off all power to the equipment.
  2. Remove doors, covers, trims, and/or dead fronts to access the I-Line interior.
  3. Turn the fused disconnect switch of the I-Line Enable Module off. Position the I-Line Enable Module jaws against the bus bar stack so the guide rib on the bottom of the I-Line Enable Module is oriented towards the alignment groove in the bus insulator base, and make sure the fingers of the I-Line Enable Module bracket fit into the key slots in the pan.

    I-Line Enable Module Positioning

  4. Place a long-shanked slotted screwdriver through the rectangular hole in the I-Line Enable Module mounting bracket and into the screwdriver slot in the mounting pan.
  5. Ratchet the I-Line Enable Module firmly onto the bus bar stack and align the retaining screw with the 7/32 in. (5.6 mm) mounting hole in the pan.
    NOTE: Do not force the I-Line Enable Module onto the bus stack.

    Ratchet the I-Line Enable Module

  6. Tighten the retaining screw securely to prevent the I-Line Enable Module from moving.

    Torque the screw to 3 N•m (20 lb-in).

    NOTE: Ensure the retaining screw is tight, but do not tighten it enough to bend the mounting bracket.

    Tighten Retaining Screw

  7. Make all necessary electrical and communication connections. Refer to Appendix A - System Communication Schematics and Appendix B - Installation Schematics for appropriate connections.
  8. Reinstall interior dead front, trim barriers, and the door pans (when applicable).
  9. Re-energize the equipment.
  10. Turn the fused disconnect switch of the I-Line Enable Module on.
    NOTE: I-Line Enable Modules are supplied with factory-applied joint compound on the plug-on connectors. The compound must not be removed because it contributes to the overall performance of the connection.
    NOTE: Whenever an I-Line Enable Module is removed and reinstalled, the joint compound must be reapplied. Use joint compound PJC-7201. A two-ounce container of this compound especially formulated for I-Line plug-on connectors is available for purchase (catalog number PJC-7201).

I-Line Enable Module Installation Graphics

I-Line Enable Module Installation

Legend — Graphics

A

Mounting Bracket Retaining Hook (fingers)

B

Pan Key Slots

C

Retaining Screw

D

Mounting Bracket

E

I-Line Enable Module Rectangular Hole

F

Guide Rib

G

Alignment Grove

I-Line Enable Module Basic Dimensions

I-Line Enable Module

Wide side version shown.

I-Line Enable Module Basic Dimensional Diagrams

Wide side version shown.

I-Line Enable Module Basic Dimensions

 

A1

A2

A3

A4

B1

B2

C1

C2

C3

C4

D1

Wide Side

inch

4.25

7.04

6.28

1.54

3.00

6.00

4.24

7.07

7.5

8.47

14.86

mm

108

179

160

39

76

153

108

180

191

215

378

Narrow Side

inch

2.74

5.52

4.77

1.54

3.00

6.00

4.24

7.07

7.5

8.47

11.83

mm

70

140

121

39

76

153

108

180

191

215

301

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.