JYT97577–01

Wiring Connection

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm that all power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • Qualified persons performing diagnostics or troubleshooting that require electrical conductors to be energized must comply with NFPA 70 E—Standard for Electrical Safety Requirements for Employee Workplaces and OSHA Standards—29 CFR Part 1910 Subpart S—Electrical.
Failure to follow these instructions will result in death or serious injury.

NOTICE
HAZARD OF FALSE TORQUE INDICATION
  • Do not allow conductor strands or wire insulation to interfere with threads of wire binding screw(s).
Failure to follow these instructions can result in equipment damage.

Connector Usage Information

Connector

Description

Conductor

Strip Length

Torque

Notes

Type

Qty

Size

Terminal Block — Multiple Poles

Al

1 per pole

24 AWG–14 AWG

(0.2–2.5 mm²)

0.28 in.

(7 mm)

4.43–5.31 lb-in

(0.5–0.6 N•m)

Two conductors, with the same cross section, may be used per pole by utilizing TWIN ferrules with plastic sleeve and having a combined cross section between 2x24 AWG–2x18 AWG (0.5–1.5 mm²).

Cu

1 per pole

RJ45–RJ45 Inline Coupler (Shielded)

Cu

Up to 8 wires (or 4 pairs)

Cat 5e

(28–22 AWG)

N/A

N/A

These connectors are used for various protocol connections. Refer to specific catalog type and location information for details.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.