JYT97577–01

Safety Packages

Maintenance Mode Setting (MMS) Switch I-LEM Package Accessory and Control Wiring

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm that all power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • Qualified persons performing diagnostics or troubleshooting that require electrical conductors to be energized must comply with NFPA 70 E—Standard for Electrical Safety Requirements for Employee Workplaces and OSHA Standards—29 CFR Part 1910 Subpart S—Electrical.
  • Proper use of MMS (Maintenance Mode Switch) requires engineering analysis, appropriate PPE, and safe electrical work practices.
  • See Instruction Bulletin MFR70008 for additional information and hazard messages.
Failure to follow these instructions will result in death or serious injury.

MMS I-LEM Switch Catalog Numbers

Catalog Number

Voltage VAC

Features

ICNL2222MMS

120–240

Narrow Side, Bottom Feed, Maintenance Mode Switch

ICNR2222MMS

120–240

Narrow Side, Top Feed, Maintenance Mode Switch

ICNL2422MMS

277–480

Narrow Side, Bottom Feed, Maintenance Mode Switch

ICNR2422MMS

277–480

Narrow Side, Top Feed, Maintenance Mode Switch

ICWL2222MMS

120–240

Wide Side, Bottom Feed, Maintenance Mode Switch

ICWR2222MMS

120–240

Wide Side, Top Feed, Maintenance Mode Switch

ICWL2422MMS

277–480

Wide Side, Bottom Feed, Maintenance Mode Switch

ICWR2422MMS

277–480

Wide Side, Top Feed, Maintenance Mode Switch

ICWL2622MMS

480–600

Wide Side, Bottom Feed, Maintenance Mode Switch

ICWR2622MMS

480–600

Wide Side, Top Feed, Maintenance Mode Switch

MMS I-Line Enable Module

MMS I-LEM System Characteristics

G1

Accessory Panel

Location of accessory operation connections

G2

24 VDC Output - PCB Connector. Phoenix Contact 1778043

Provides 24 VDC from Power Supply to the Trip Unit

G3

PCB Connector Multiple Poles. Phoenix Contact 1757019

Connections for MMS Switch to MicroLogic Trip Unit ZSI terminals

G4

MMS (Maintenance Mode Setting) Switch

Switch for activation "ON" / deactivation "OFF" of MMS function

G5

2-Pole Fused Disconnect Switch

Provides the ability to remove power from the inside of the unit while installed on the I-Line bus stack or connected to the LINE side power source. It doesn't remove power from I-Line bus stack. Fuses: 5A, FNQ-R-5 CC

NOTE: Refer to Connector Usage Information for connector details.

MMS I-LEM Accessory Panel

MMS I-LEM Accessory Panel Connection Identification

P

24 VDC Power Outputs Connections

24 AWG–14 AWG (0.2–2.5 mm²) twisted pair cable

Z

ZSI Connections (Z3 and Z4)

24 AWG–14 AWG (0.2–2.5 mm²) twisted pair cable

MMS I-LEM Connections

NOTE: Refer to the Maintenance Mode Switch Instruction Bulletin (MFR70008) for operation and testing instructions.

  1. Locate the circuit breaker that will be using the MMS. The intended circuit breaker must be within visual range of the switch (MMS functions with trip units that have the Short-time Zone Selective Interlocking (ST-ZSI) capability).
  2. Install the MMS I-Line Enable Module according to the I-Line Enable Module installation instructions.
  3. Prepare the intended circuit breaker. Follow the instructions provided with the circuit breaker for all PPE, safe electrical work practices, and hazard messages.
    1. Remove the plastic cover of the circuit breaker (P- or R-Frame). The number of fasteners will vary depending on the frame size of the circuit breaker.
    2. Remove the connector block from the top of the trip unit.
    3. Locate the "Z" connections of the trip unit (typically the left-most section of the 12-pole connector located on the top of the trip unit).
    4. Provide wires from the Z3 and Z4 connections and route them through the wiring conduit provided on the left-most portion of the molded case of the circuit breaker. Provide a 2 in. jumper between the Z5 and Z3 connection locations. Refer to Connector Usage Information for wire size and strip length details. (The wire length should be in excess of the wire-routing path distance from the circuit breaker to the MMS I-Line Enable Module).
    5. You can also provide 24 VDC power to the trip unit by connecting to the "F" connections (typically the right-most section of the 12-pole connector located on the top of the trip unit).
    6. Provide wires from the F1 and F2 connections and route them through the wiring conduit provided on the left-most portion of the molded case of the circuit breaker. Refer to Connector Usage Information for wire size and strip length details. (The wire length should be in excess of wire-routing path distance from the circuit breaker to the MMS I-Line Enable Module).
    7. Replace the connector on the top of the trip unit.
    8. Replace the plastic cover of the circuit breaker.
  4. Connect the wires from Z3 and Z4 (described in step 3-d above) to the MMS I-Line Enable Module ZSI connections (refer to GDE8239900—MMS I-Line Enable Module (240, 480, and 600 VAC) for location). Refer to Connector Usage Information for wire size and strip length details.
  5. Connect the wires from F1 and F2 (described in step 3-f above) to the MMS I-Line Enable Module 24 VDC output connections (refer to GDE8239900—MMS I-Line Enable Module (240, 480, and 600 VAC) for location). Refer to Connector Usage Information for wire size and strip length details.

Energy Reduction Maintenance Setting (ERMS) I-LEM Accessory and Control Wiring

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm that all power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • Qualified persons performing diagnostics or troubleshooting that require electrical conductors to be energized must comply with NFPA 70 E—Standard for Electrical Safety Requirements for Employee Workplaces and OSHA Standards—29 CFR Part 1910 Subpart S—Electrical.
  • Proper use of ERMS (Energy Reduction Maintenance Setting) switch requires engineering analysis, appropriate PPE, and safe electrical work practices.
  • Refer to Instruction Bulletin NHA67346 for additional information and hazard messages.
Failure to follow these instructions will result in death or serious injury.

ERMS I-LEM Catalog Numbers

Catalog Number

Voltage VAC

Features

ICWL2222ERMS

120–240

Wide Side, Bottom Feed, ERMS - Ethernet communications

ICWR2222ERMS

120–240

Wide Side, Top Feed, ERMS - Ethernet communications

ICWL2422ERMS

277–480

Wide Side, Bottom Feed, ERMS - Ethernet communications

ICWR2422ERMS

277–480

Wide Side, Top Feed, ERMS - Ethernet communications

ICWL2222ERM2

120–240

Wide Side, Bottom Feed, ERMS - Modbus communications

ICWR2222ERM2

120–240

Wide Side, Top Feed, ERMS - Modbus communications

ICWL2422ERM2

277–480

Wide Side, Bottom Feed, ERMS - Modbus communications

ICWR2422ERM2

277–480

Wide Side, Top Feed, ERMS - Modbus communications

ICWL2622ERM2

480–600

Wide Side, Bottom Feed, ERMS - Modbus communications

ICWL2622ERM2

480–600

Wide Side, Top Feed, ERMS - Modbus communications

NOTE: ERMS units are to be used with X.0 P or H level MicroLogic trip units with ERMS blue label.

ERMS IFE I-Line Enable Module

ERMS IFM (ERM2) I-Line Enable Module

NOTE: Ethernet Version shown. Modbus version contains multiple IFMs rather than an IFE. ERMS Switch position is subject to change for clearance purposes without effect.

ERMS I-LEM System Characteristics

A1

Accessory Panel

Location of accessory operation connections.

A2

Local Ethernet - RJ45 Connector (Bulkhead)

Front Ethernet access to IFE module for initial set-up or monitoring. Temporary use only. (Not available for IFM I-LEM versions).

A3

Ethernet - RJ45 Connector Commscope 2111122-1

Ether 1 - Ethernet connection for remote set-up and monitoring of the ERMS function.
Ether 2 - For daisy chaining other I-Line Enable Module units or Ethernet communicating equipment.

A4

ULP - RJ45 Connector Commscope 2111122-1

NSX cord connection(s) for ULP communications with circuit breaker(s). (Note: 600 V I-Line Enable Module maximum capacity is quantity 1 ULP port.)

A5

RS-485 (2-wire Modbus)  - RJ45 Connector. Commscope 2111122-1

RS-485 port for daisy chaining other I-Line Enable Module units or Modbus communicating equipment for Modbus-SL network connection. (IFM Version Only).

A6

2-Pole Fused Disconnect Switch

Provides the ability to remove power from the inside of the unit while installed on the I-Line bus stack or connected to the LINE side power source. It doesn't remove power from I-Line bus stack.

A7

I/O Module Schneider LV434063

Provides ability to switch trip unit to ERMS setting function. The ERMS system is programmed to default to an Instantaneous (Ii setting) of 2 x In.

A8

IFE Ethernet Switchboard Server Schneider LV434002

Enables the I-Line Enable Module (therefore the circuit breaker) to be connected to an Ethernet network. (IFE Version Only).

A9

IFM Modbus-SL Interface Schneider LV434000

Enables the I-Line Enable Module (therefore the circuit breaker) to be connected to an RS-485 Serial Line Modbus network and ULP to Modbus-SL converter. (IFM Version Only).

A10

ERMS Switch Assembly (Padlockable Cover)

Manual switch to turn the ERMS setting ON/OFF. When the ERMS switch is “ON” the trip unit (circuit breaker) is in maintenance mode. The trip unit is in ERMS mode when the ERMS switch is lit.

A11

24 VDC Output - PCB Connector. Phoenix Contact 1757019

Provides 24 VDC from the power supply to the trip unit.

NOTE: Refer to Connector Usage Information for connector details.

ERMS IFE I-LEM Accessory Panel

ERMS IFM (ERM2 I-LEM) Accessory Panel

ERMS I-LEM Accessory Panel Connection Identification

P

24 VDC Power Outputs Connections

24 AWG–14 AWG (0.2–2.5 mm²) twisted pair cable

E

Ethernet Connections. (IFE Version Only)

Cat 5e Shielded

1

ULP 1 – IFE. (IFE Version Only)

Cat 5e Shielded

R

RS-485 Connection, 2-wire Modbus. (IFM Version Only)

Cat 5e Shielded

1

ULP 1 – IFM 01. (IFM Version Only)

Cat 5e Shielded

2

ULP 2 – IFM 02. (IFM Version Only)

Cat 5e Shielded

3

ULP 3 – IFM 03. (IFM Version Only)

Cat 5e Shielded

4

ULP 4 – IFM 04. (IFM Version Only)

Cat 5e Shielded

ERMS I-LEM and ERM2 I-LEM Connections

NOTE: Refer to the bulletins shipped with each component and included in the I-Line Enable Module installation packet for detailed set-up instructions.

  1. Install the ERMS I-Line Enable Module according to the I-Line Enable Module installation instructions.
  2. Connect 24 VDC power wires from the MicroLogic trip unit in the circuit breaker to the 24 VDC power supply connector on the accessory panel of the ERMS I-Line Enable Module. See Connector Usage Information.
    NOTE: Refer to the instructions provided with the circuit breaker and/or trip unit for details.
  3. Connect the RJ45 end of the NSX cord from the circuit breaker BCM (Breaker Communication Module) or BSCM (Breaker Status Control Module) to the RJ45 connector labeled "ULP" on the accessory panel of the I-Line Enable Module. See ERMS I-LEM System Characteristics for additional details.
  4. For ERMS Unit (Ethernet TCP version): Connect the Ethernet cable to the RJ45 connector labeled "ETHER 1" on the accessory panel for remote set-up or monitoring of the ERMS I-Line Enable Module.

    Optional: A second RJ45 connector, labeled "ETHER 2," is available for daisy chaining a U-PaS I-Line Enable Module (in conjunction with an IFM unit to provide communication to other communicating circuit breakers), or for daisy chaining Ethernet communicating equipment.

    Refer to ERMS I-LEM Communication Schematic Diagram and NVE4858900—ERMS I-Line Enable Module (240 and 480 VAC) .

  5. For ERM2 Unit (ERMS Modbus Serial version): Connect the Modbus Serial cable to the RJ45 connector labeled "RS-485" on the accessory panel for remote set-up or monitoring of the ERM2 I-Line Enable Module. Additional ULP connectors are available to provide communication to other communicating circuit breakers as needed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.