JYT97577–01

Metering Packages

Power Meter I-LEM Series Package Accessory and Control Wiring

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm that all power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • Qualified persons performing diagnostics or troubleshooting that require electrical conductors to be energized must comply with NFPA 70 E—Standard for Electrical Safety Requirements for Employee Workplaces and OSHA Standards—29 CFR Part 1910 Subpart S—Electrical.
Failure to follow these instructions will result in death or serious injury.

Power Meter I-LEM Series Catalog Numbers

Catalog Number

Voltage VAC

Features

ICWL243X5563

120-480

Wide Side, Bottom Feed, PM5563 meter

ICWR243X5563

120-480

Wide Side, Top Feed, PM5563 meter

ICWL243X8244

120-415

Wide Side, Bottom Feed, PM8244 meter

ICWR243X8244

120-415

Wide Side, Top Feed, PM8244 meter

ICWL263X5563

480-600

Wide Side, Bottom Feed, PM5563 meter

ICWR263X5563

480-600

Wide Side, Top Feed, PM5563 meter

ICWL263X8244

480-600

Wide Side, Bottom Feed, PM8244 meter

ICWR263X8244

480-600

Wide Side, Top Feed, PM8244 meter

Power Meter Series I-Line Enable Module

Power Meter I-LEM Series System Characteristics

D1

Accessory Panel

Location of accessory operation connections.

D2

Local Ethernet -  RJ45 Connector (Bulkhead)

Front Ethernet access to Power Meter for initial set-up or monitoring. Temporary use only.

D3

Ethernet - RJ45 Connector Commscope 2111122-1

Ether 1 - Ethernet connection for remote set-up and network connection.
Ether 2 - For daisy chaining other I-Line Enable Module units or Ethernet communicating equipment.

D4

RS-485 (2-wire Modbus)  - RJ45 Connector. Commscope 2111122-1

RS-485 port for daisy chaining to other I-Line Enable Module units or Modbus communicating equipment for Modbus-SL network connection.

D5

Current Transformer (CT) signals - PCB Connector. Phoenix Contact 1825527

CT connections for meter (A, B, C phases and current flow (In) in the neutral conductor).

D6

Digital Input / Digital Output signals - PCB Connector. Phoenix Contact 1825569

Provides connection to 2 Digital Inputs and 2 Digital Outputs

D7

Power Meter (PM Series) and Power Meter Remote Display

Power Meter (refer to meter documentation for detailed capabilities.)
PM5563: Basic Power Meter + Remote Meter Display
PM8244: Intermediate Power Meter + Remote Meter Display

D8

3-Pole Fused Disconnect Switch

Provides the ability to remove power from the inside of the unit while installed on the I-Line bus stack or connected to the LINE side power source. It doesn't remove power from I-Line bus stack.

D9

Voltage Neutral (VN) Input - PCB Connector Phoenix Contact 1825501

Voltage neutral connector: VN input for voltage measurement (when neutral is present)

Power Meter I-LEM Series Accessory Panel

Power Meter I-LEM Accessory Panel Connection Identification

CI

Current Inputs (CT Connections)

4-pin plug-in connector (From shorting block connector 14 AWG)

E1

Ethernet 1 Connection (Output typical)

Cat 5e Shielded—RJ45

E2

Ethernet 2 Connection (Input typical)

Cat 5e Shielded—RJ45

R

RS-485 Modbus-SL or BACnet Connection

Cat 5e Shielded—RJ45

VN

Voltage Neutral Connection (as required)

14 AWG (2.5 mm²) wire

X

D1/D2 Output Connections

24 AWG (0.2 mm²) twisted pair

Y

S1/S2 Input Connections

24 AWG (0.2 mm²) twisted pair

Power Meter I-LEM Package Connections

NOTE: Refer to the bulletins shipped with each component and included in the I-Line Enable Module installation packet for detailed set-up instructions.

  1. Install the power meter shorting block (included in package), according to the instructions provided, prior to installing the Power Meter I-Line Enable Module.
  2. Install Power Meter I-Line Enable Module according to the I-Line Enable Module installation instructions.
  3. When connecting the CTs to the shorting block of the Power Meter I-Line Enable Module, note that typically "X1"="White"="+" and "X2"="Black"="-". However, refer to the CT manufacturer’s specifications for the exact nomenclature equivalent to primary "X1" and secondary "X2."
  4. If the system uses an alarm output or additional inputs, connect to the appropriate Input/Output terminals on the accessory panel of the Power Meter I-Line Enable Module identified as X = D1/D2 (Outputs) and Y =S1/S2 (Inputs).
  5. If the voltage system requires a neutral, a connection must be made from the panelboard neutral to the terminal identified as "VN" on the accessory panel in the Power Meter I-Line Enable Module.
  6. Connect the Ethernet cable to the RJ45 socket connector labeled "ETHER 1" on the accessory panel for remote set-up or monitoring of the Power Meter I-Line Enable Module.

    Optional: A second Ethernet RJ45 connection, labeled "ETHER 2," is available for daisy chaining additional Power Meter I-Line Enable Modules, or for daisy chaining Ethernet communicating equipment.

    Refer to Power Meter I-LEM Communication Schematic Diagram and Metering Packages - Installation Schematics.

  7. If communicating circuit breakers are present in the same system with the Power Meter, they are interconnected to the communication system via an IFM I-Line Enable Module in conjunction with a U-PaS I-Line Enable Module.

    Connect the Ethernet cable to the RJ45 connector (labeled "ETHER 1") on the accessory panel of the Power Meter I-Line Enable Module and to the RJ45 connector (labeled "ETHER 2") on the U-PaS I-Line Enable Module to daisy chain the two devices.

    Connect the Ethernet cable to the RJ45 connector labeled "ETHER 1" on the U-PaS accessory panel for remote set-up or monitoring of the network.

    Connect the Modbus Serial cable to the RJ45 connector labeled "RS-485" on the U-PaS accessory panel for daisy chaining an IFM I-Line Enable Module. This connection allows the system to feature ULP connections to provide communication to communicating circuit breakers.

    Refer to Power Meter I-LEM Communication Schematic Diagram, Power Meter I-LEM with Communicating Circuit Breakers Communication Schematic Diagram, and Metering Packages - Installation Schematics.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.