JYT97577–01

NSX Cord

A shielded communication cable consisting of two twisted pairs of stranded wire that is typically black/red and blue/white color. The NSX Cord has an RJ45 jack at one end, and four wires terminated into a small terminal block on the other end. This is used with PowerPacT H, J, or L breakers. If the terminal block is not needed, it can be removed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.