JYT97577–01

General Information

Introduction

This bulletin contains instructions for installing Square D brand I-Line Enable Modules. These I-Line Enable Modules are Underwriters Laboratories (cURus) approved and are suitable to be installed in I-Line Panelboards or QED2 I-Line Distribution Sections.

Assistance

For technical support on the installation of this I-Line Enable Module, contact Schneider Electric customer support at 1–888–778–2733.

Refer to https://www.se.com.

Kit Contents / Necessary Tools

Kit Contents and Necessary Tools

Small screwdriver
(blade 0.4 x 2.5 mm)

Wire strippers

I-Line Enable Module (Wide Side version shown)

#2 Phillips screwdriver

Long-shanked flat head screwdriver

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.