JYT97577–01

I-Line Enable Definition

I-Line Enable Modules are a range of I-Line stack-mounted modular units. The modular unit is a mechanical and electrical assembly containing one or more devices to perform a function in a panelboard (or switchboard). Its built-in electronics and devices are suited for monitoring, metering, communication, and protection features.

With the footprint of an L-Frame PowerPacT Circuit Breaker, all I-Line Enable Modules mount inside a standard panelboard to provide a compact, space saving installation.

The product name “I-Line Enable Module” (also called “I-LEM”) applies to both the enclosure and the device with which it is provided and gives it the name.

For the fullest description and technical characteristics of devices, refer to the related documents listed in Appendix C - Documentation References.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.