Device Logging
Description
Logging is available for the devices which are in the device list. The logging contents can be customized using topics. Topics are the parameters for a device that can be selected to have the desired logging content. The number of log entries per device is fixed irrespective to the number of topics selected for that device. The IFE server can log data received at predefined intervals (5, 10, 15, 20, 30, and 60 minutes). Below is an explanation of how the IFE server logs data and how to set up logging for a device.
Logging Interval
Many devices in a power monitoring system do not have the ability to record data in non-volatile memory. The IFE server provides this data logging at predefined intervals for up to 13 devices.
The features of IFE data logging are:
-
The maximum number of log entries per device is fixed to 12960.
-
Select maximum of 13 devices for data logging.
-
Select maximum of 24 topics per device for data logging (topics are kVAh, kWh, kVARh, and so on).
-
Select the desired device and list of topics for data logging.
Logging interval is a predefined time for the IFE server to log data received from the device. The logging capacity of a device is calculated by multiplying the log capacity factor with the logging interval set in the page.
Logging capacity (in days) = Log capacity factor * logging interval (in minutes)
The log capacity factor is 9 and is calculated as follows:
Log capacity factor = 12960/1440
Where:
-
12960 is the maximum number of log entries per device
-
1440 is the number of minutes per day
Example: If the in the page is set to 5 minutes, then the logging capacity is 45 days.
The table shows the logging capacity for the corresponding logging interval:
|
Logging Interval (Minutes) |
Logging Capacity (Days) |
|---|---|
|
5 |
45 |
|
10 |
90 |
|
15 |
135 |
|
20 |
180 |
|
30 |
270 |
|
60 |
540 |
Interval Logging Setting Procedure
Each device in the device list may be independently enabled for logging. Topics to log are unique to each device. To view interval data logs, refer to Device Logging in menu.
Logging
To disable logging, select the logging interval as , ensure that the logging selections are cleared, then click .
Purge Data
To delete a data log, check for the topics to be deleted.
Customize
To customize logging content, enable device logging. Click under for the device to be configured.