Modbus TCP/IP Filtering
Description
The page allows you to define the level of access for Modbus TCP/IP clients connected to IFE server.
Block Connections
You can select the maximum number of IP connections allowed, 8 or 16. Each connection can have 12 concurrent transactions simultaneously.
If IP Filtering is enabled, you must configure the IP address of the PC in the list of allowed addresses with read/write permission for using the EcoStruxure Power Commission software.
IP Filtering
|
Parameter |
Description |
Setting |
|---|---|---|
|
|
Activates the IP address filtering. The list of IP addresses available in the table is granted access. |
|
|
|
Filters the required IP address entered by you. |
10 addresses (Maximum allowed IP addresses) |
|
|
Defines the access level for the corresponding IP address. |
|
|
|
Allows all Modbus TCP/IP clients to have the read-only access. |
|