Device List
Description
The IFE server (ULP port, serial port) and remote Modbus/TCP slave devices. In the device list, you can add, delete and/or discover devices.
page is used to define the list of devices connected to theThe list of connected devices is defined by either of the following:
-
Automatically, by using the device discovery procedure
-
Manually, by adding the devices one by one.
Number of Modbus Slave Devices
A maximum of 20 slave devices can be added in the device list. Under each IFE server or master remote device, a maximum of 11 IFM interfaces can be added.
The application dictates the maximum slave devices or IFM interfaces that can be used. The following general guidelines can be used to size the application:
-
Maximum of 20 slave devices are technically supported via the IFE webpages.
-
Maximum of 11 IFM interfaces can be physically connected to one IFE server. This can be used for applications that have the lowest performance requirement and are recommended for simple applications.
-
Maximum of 8 IFM interfaces should be used for applications that requires regular access via the IFE webpages or that have other masters communicating, such as FDM128 display. This normally provides a reasonable response time for up to three masters.
-
The number of IFM interfaces that can be stacked in a more complex environment, for example, with SCADA or Building Management Systems must be scaled to the performance needs in the application.
Device List Parameters
Parameters |
Description |
Settings |
---|---|---|
|
Displays the device IP address.
|
– |
|
Indicates if the IP device is a gateway or not.
|
check box is always selected. |
|
Displays the Modbus slave address of the IFE server and the remote device.
|
|
|
Allows you to enter the names for IFE server and remote device. NOTE:
|
The IFE name can have up to 64 ASCII characters with the following characters: A–Z, a–z, 0–9, and -. However, - cannot be used at the end of the name. NOTE:
|
|
Displays the connection type. It is unavailable to edit. |
The 2 types of port are:
|
|
Allows you to select the slave devices from the list of supported devices. |
– |
|
Allows you to enter the name for the discovered devices.
NOTE: Delete and edit operations are not allowed
if the device is selected for logging.
|
The device name can have up to 64 ASCII characters with the following characters: A–Z, a–z, 0–9, and -. However, - cannot be used at the end of the name. |
|
Displays the local address of the device connected to the IFE server or remote device. |
|
|
Allows you to add remote devices. |
– |
|
Allows you to save device list configuration. |
– |
|
Allows you to delete the selected slave devices. NOTE: Delete operation is not allowed
if the device is selected for logging.
|
– |
|
Allows you to discover the slave devices. NOTE: The
button for the remote device is available only if you
click the button.NOTE: The discover option for the device type BCM-OF/SD
is available only on IFE’s own IMU.
|
– |
Allows you to add a new slave device to the device list. |
– |
|
|
Allows you to delete the remote device. NOTE: Delete operation is not allowed if the
device is selected for logging.
|
– |
Adding Device to the Device List for the First Time
Step |
Action |
Result |
---|---|---|
1 |
Slave device to IFE server: Add the slave devices to the IFE server manually or by device discovery. |
Adds the slave device to IFE server. |
2 |
Remote device: In the page, click to add a remote device. |
Adds the remote device in the page. |
3 |
Slave device to remote device: Add the slave device for remote device by device discovery. NOTE: The
button for the remote device is available only if you
click the button. |
Adds the slave device to remote device. |
4 |
Repeat step 2 and 3 to add more remote devices to page.Click to save the modified changes. |
– |
Device Discovery Procedure
When you start device discovery, the IFE server queries the ULP port, serial port, and Ethernet port using a user-defined address range. Modbus RTU protocol is used for discovery on the serial port. If the device replies to the query, the local ID is set to the current discovery address, and the device is given a default device name. The IFE server, then tries to identify the device type. If the IFE server recognizes the device type of the discovered device, the IFE server sets the recognized device type in the field. If the IFE server does not recognize the of the discovered device, the IFE server sets to Modbus in the field.
The list of devices supported by the IFE server is in Appendix.
The table shows the steps to add device using device discovery procedure:
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the menu. |
2 |
From the menu, in the submenu, click . |
Opens the page. |
3 |
To discover locally connected devices, click . |
Opens the page. |
4 |
Enter and . |
Enters the discovery address range. |
5 |
Click . (Click to stop the process).NOTE: Discovery only finds local serial Modbus devices connected to the IFE server. The device on the ULP port
is discovered automatically.
|
Begins to discover all connected devices. |
6 |
Enter a new device name in the text box. |
Renames the device. |
7 |
Select the check box for the device to be saved in the device list. |
Selects or deselects a device entry to be saved or removed. |
8 |
Click in the page. |
Displays the saved device list. |
Device Discovery Parameters
Parameters |
Description |
Setting |
---|---|---|
|
Defines the Modbus slave address range that is to be used to discover devices on the IFE serial port. |
|
|
Allows you to save the selected device to the . |
– |
|
Displays the IP address of the IFE server or the remote device. |
– |
|
Lists the device type that was defined for this device. |
– |
|
Allows you to assign the device type from the drop-down list. |
– |
|
Allows you to enter a custom name for the device. |
– |
|
The slave address of the device connected to the IFE server. |
– |
|
Displays the discovery or validation status. |
|
Adding a Device Manually
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the menu. |
2 |
From the menu, in the submenu, click . |
Opens the page. |
3 |
Allows you to add device in the device list. |
|
4 |
Choose the supported device from the list. |
Selects the device type selected from the list. |
5 |
Enter a new device name in the text box. |
Renames the device. |
6 |
Enter the local address of the device in the text box. |
Displays the local address of the device. |
7 |
Click . |
A new device is added to the list. |