1040IB1401-10

IMU Information

Description

The IMU Information page gives the information about the devices which are connected to the ULP port of the IFE server. The devices connected are:

  • BCM ULP module

  • MicroLogic trip unit

  • BSCM module

  • FDM121 display

  • IO module IO 1

  • IO module IO 2

  • UTA module

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?