Firmware Update
Description
Use the latest version of EcoStruxure Power Commission software for all firmware updates.
The latest version of IFE firmware and IFE webpages are updated in a single operation through EcoStruxure Power Commission software.
For more information on IFE firmware versions, refer to Enerlin'X IFE Server Firmware Release Note.
WARNING |
|---|
|
LOSS OF DATA
Backup the data log files before updating the firmware.
The data log entries of the IFE server
may be lost when the IFE firmware
is updated.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
After updating the firmware of one device in the IMU, use the latest version of EcoStruxure Power Commission software to check the firmware compatibility between the IMU devices. The Firmware Update table helps you to diagnose and identify all discrepancy issues between the IMU devices. This table also provides the recommended actions relevant to the detected discrepancies.
Checking the Firmware Version
You can find the firmware version of the devices in the IMU by using:
-
EcoStruxure Power Commission software, refer to the EcoStruxure Power Commission Online Help
DOCA0069EN. -
IFE webpages, see the procedure below.
|
Step |
Action |
Result |
|---|---|---|
|
1 |
Open the web browser and log in to the IFE webpage. |
Opens the IFE home page. |
|
2 |
Locate the firmware version on page on the menu Device Identification. NOTE: If you
have updated the firmware recently, press to refresh the webpage and
update the displayed firmware number.
|
Determines the firmware version of the IFE server. |
Updating the Firmware and Webpages, Using EcoStruxure Power Commission Software
For more information, refer to the EcoStruxure Power Commission Online Help
The EcoStruxure Power Commission software is available at www.se.com.
WARNING