Set Device Time
Description
The page allows you to synchronize the date and time of the slave devices connected to the IFE server to IFE date and time. It also allows you to get the device time that are connected to the IFE server. This page lists the slave devices that require an external interface to set their date and time.
List of Parameters in Set Device Time
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the device from the list for synchronizing, getting, and synchronizing the time. |
|
|
Displays the time of the selected device. |
|
|
Displays the status of the selected device. |
|
|
Allows you to get the time of the selected device. |
|
|
Allows you to set the time of the selected device. |
Setting the Device Time
|
Step |
Action |
Table |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, click . |
Opens the page. |
|
3 |
Select the devices from the page, and then click . |
The selected slave device date and time gets synchronized with the IFE time and the status is updated as successful. NOTE: If the selected device fails to synchronize with IFE date and time, then the status is updated as unsuccessful.
NOTE: feature is not applicable for IFE’s own IMU and shows the set status as (Not Applicable).
|