1040IB1401-10

Schematics with MasterPact MTZ Circuit Breakers

Description

FYI, this map is shared by IFE user guide and MTZ Modbus guide.

The IFE server is connected to the MasterPact MTZ circuit breaker through its ULP port module.

For more information, refer to the ULP System User Guides .

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to an RJ45 ULP port.
  • The RJ45 ULP ports of IFE server are for ULP modules only.
  • Any other use can damage the IFE server or the device connected to the IFE server.
  • To check if an ULP module is compatible with the RJ45 ULP ports of IFE server, refer to the ULP System User Guides.
Failure to follow these instructions can result in equipment damage.

All the connection configurations require the RJ45 male/male ULP cord.

When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A

RJ45 male/male ULP cord

B

ULP line termination

Connection of the IFE Server to a MasterPact MTZ Circuit Breaker

Connect the IFE server to the ULP port module on a MasterPact MTZ circuit breaker by using the ULP cord.

A

IFE Ethernet switchboard server

B

ULP line termination

C

RJ45 male/male ULP cord

D

ULP port module

E

MasterPact MTZ fixed circuit breaker

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?