Introduction
Overview
The IFE Ethernet switchboard server (or IFE server) enables an intelligent modular unit (IMU) with a ComPact™, PowerPact™, or MasterPact™ circuit breaker to be connected to an Ethernet network. Each circuit breaker has its own IFE server and a corresponding IP address.
The IFE server with part number LV434002 is an Ethernet switchboard server for ComPact, PowerPact, and MasterPact circuit breakers and a server for Modbus-SL (serial line) connected devices.
IFE Server Features
The main features of IFE server are:
-
Dual Ethernet port for simple daisy chain connection
-
Device profile web service for discovery of the IFE server on the local area network (LAN)
-
ULP compliant for location of the IFE server in the switchboard
-
Ethernet interface for ComPact, PowerPact, and MasterPact circuit breakers
-
Server for Modbus-SL connected devices
-
Embedded setup webpages
-
Embedded monitoring webpages
-
Embedded control webpages
-
Built-in email alarm notification for circuit breaker connected to IFE server.