Schematics with PowerPacT H-, J-, and L-Frame Circuit Breakers
General Description
Depending on the configuration of the PowerPacT H-, J-, and L-frame circuit breaker, connect the IFE server to the circuit breaker using one of the following configurations:
-
Connection of the IFE server to the MicroLogic trip unit
-
Connection of the IFE server to the BSCM module
-
Connection of the IFE server to the BSCM module and to the MicroLogic trip unit
For more information, refer to the ULP System User Guide.
ULP Connection
![]() |
---|
HAZARD OF ELECTRIC SHOCK
For system voltage greater than 480 Vac:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
NOTICE |
---|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All connection configurations require the NSX cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.
When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A |
NSX cord or RJ45 male/male ULP cord |
B |
ULP line termination |
Connection of the IFE Server to the MicroLogic Trip Unit

A |
IFE Ethernet switchboard server |
B |
ULP line termination |
C |
NSX cord |
D |
MicroLogic trip unit |
Connection of the IFE Server to the BSCM Module

A |
IFE Ethernet switchboard server |
B |
ULP line termination |
C |
NSX cord |
D |
BSCM breaker status control module |
Connection of the IFE Server to the BSCM Module and to the MicroLogic Trip Unit

A |
IFE Ethernet switchboard server |
B |
ULP line termination |
C |
NSX cord |
D |
BSCM breaker status control module |
E |
MicroLogic trip unit |
Connection of the IFE Server to a Circuit Breaker for System Voltage Greater Than 480 Vac

A |
IFE Ethernet switchboard server |
B |
ULP line termination |
C |
RJ45 male/male ULP cord |
D |
Insulated ULP module for system voltage greater than 480 Vac |
E |
Insulated ULP cord for system voltage greater than 480 Vac |
F |
Connector for PowerPact H-, J-, and L-frame Circuit Breakers internal connection |