1040IB1401-10

Indicators

Description

The Indicators page provides the maintenance counter information for the selected device. The page displays the information about the remaining service life of the circuit breaker, contact wear counters, circuit breaker operation counters, and the cradle counters.

Viewing Maintenance Counters

Step

Action

Result

1

From the IFE menu, click Maintenance.

Opens the Maintenance page.

2

From the Indicators menu, select the device from the device list.

NOTE: This feature is available for circuit breakers only.

Displays the information about the remaining service life of the circuit breaker, contact wear counters, circuit breaker operation counters, and the cradle counters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?