VIGED310022EN-06

Date/Time

Applicable for IM20

The date/time must be set:

  • On first power up.

  • When switching between summer and winter time and vice versa.

The date is displayed in the format: dd/mm/yyyy. The time is displayed using the 24-hour clock in the format: hh/mm.

When the device is powered up, the clock icon flashes on the system monitoring screens to indicate that the clock needs to be set. To set the date and time, see Parameter modification using the display.

NOTE: The date and time must be synchronized with the network time at the beginning of each month to ensure accurate system logging and reliable event time-stamping.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.