VIGED310022EN-06

Configuring the I/O configuration parameters

Configure the injection inhibition input and insulation alarm relay parameters using the I/O Configuration screen.

To configure the I/O configuration parameters:

  1. Select the I/O Configuration folder to open the dialog showing the list of parameters.
  2. Choose the parameters you need to modify and select Edit.

    Parameters

    Options

    Description

    Injection Inhibition Input

    Normally open

    Normally closed

    Injection exclusion is controlled by the inhibition input of the device, which is linked to the auxiliary contacts of the circuit breakers.

    Insulation Alarm Relay

    Standard connection

    failsafe

    Configure the insulation alarm relay mode based on the insulation status.

  3. Select OK, and then select Send to save your changes to the device.
    NOTE: When changes are not saved to the device, the status bar on the bottom left screen shows Download Incomplete.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.