VIGED310022EN-06

Reset

You can reset logs and trends. Further, you can perform factory reset.

You can access the device reset parameters by selecting Menu > Settings > Reset.

The reset parameters are Reset Logs, and Factory Reset.

On performing reset of logs, the existing logs information is erased but the settings parameter value remains unchanged. On performing factory reset, the settings parameter values are reset to default.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.