VIGED310022EN-06

Configuring the transformer setup

Configure the transformer parameters using the Transformer Setup screen.

To configure the transformer setup:

  1. Select the Transformer Setup to open the dialog setup.
  2. Select the CT Primary (A) and select Edit to open CT Primary (A) dialog.
  3. Select the transformer parameter from the list and edit the settings.

    Parameters

    Options

    Description

    CT Primary (A)

    40 to 9999

    (Default: 50)

    This value should match the CT installed on the primary side of the system to ensure accurate scaling of measured current.

    CT Secondary

    1 Amp

    5 Amps

    (Default: 5 Amps)

    Specifies the rated secondary current of the CT. This must match the CT’s actual secondary rating to avoid measurement errors.

    Nominal Current

    12 to 9999

    (Default: 36)

    Sets the expected operating current of the system. Used as a reference for calculating load percentage and triggering alarms.

    Threshold (%)

    1 to 100

    (Default: 80)

    Determines the load level (as a percentage of nominal current) at which warnings or alarms are activated. Helps in early detection of overload conditions.

  4. Select OK, and then select Send to save your changes to the device.
    NOTE: When changes are not saved to the device, the status bar on the bottom left screen shows Download Incomplete.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.