VIGED310022EN-06

Generating the device configuration reports

Generate reports for the current device configuration using the Reports screen. You can use this screen to view, print, and save a report file that records the device's current configuration.

To generate the device configuration reports:

  1. Select Reports to open the dialog.
  2. Select the Display to retrieve the device configuration report.
    The ION Setup retrieves and uploads report details from your device to the screen. Depending on the data, this process may take a few moments or several minutes to complete. After completion, all report parameters and their respective values will be displayed.
  3. Select Save As to save the configuration report as a .TXT file, or select Print to print the configuration report.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.