VIGED310022EN-06

Example: injection exclusion with multiple interconnected incoming feeders

By using a PLC, the wiring can be simplified and complex configurations can be considered.

The PLC can have the following characteristics:

  • Number of digital inputs: is the number of circuit breakers for incoming feeder and for coupling. These inputs can be self-powered by the PLC or powered by an external power supply.

  • Number of digital outputs: is the number of devices minus 1. These digital outputs can be electromechanical or solid-state outputs.

  • Processing cycle is equal to 0.1 s or less.

Using a basic PLC to manage device exclusion allows to:

  • Monitor continuously each part of ungrounded power system.

  • Have a short response time to detect insulation faults.

  • Be compatible with complex power systems with high number of incoming feeders and couplings.

Truth table:

Possible configurations

0 = open, 1 = closed

Injection Inhibition

0 = injection, 1 = injection inhibited

D1 D2 D3 C1 C2 IMD no.1 IMD no.2 IMD no.3
0 0 0 0 0 0 0 0
0 0 0 0 1 0 0 0
...
0 1 1 1 1 0 0 1
...
1 1 1 1 1 0 1 1

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.