VIGED310022EN-06

Log

Applicable for IM20

The device records the details of the 60 most recent insulation fault events. The fault events are triggered by one of following statuses:

  • insulation fault

  • preventive insulation fault

Event 1 is the event that was recorded most recently and event 60 is the oldest recorded event.

The oldest event is deleted when a new event occurs (the table is not reset).

By referring to this information, the performance of the distribution system can be improved and maintenance work is facilitated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.