VIGED310022EN-06

Injection inhibition screen

When the injection inhibition function is activated (that is, Inhibit. Input is set to N.O.), the following status screen displays and replaces any system status screen that may be displaying already (insulation measurement, insulation alarm or preventive insulation alarm).

You can perform the following actions on this screen:

  • Press the Menu button to go to the main menu.

  • Press the arrow buttons to view the settings screen.

  • Press the T button to run the auto-test.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.