VIGED310022EN-06

R and C measurement scenarios

The resistance and capacitance of your power system affects your device’s measurements.

The diagram below shows the insulation resistance R and the leakage capacitance C of the power system.

The following situations may occur on an installation. The gray arrows represent the preferred route for the IMD injection signal.

R and C value Equivalent circuit diagram Impact on measurements Significance of R Significance of C
R Weak (in the event of a fault) Most of the injection signal goes into R. Throughout the duration of the insulation fault, the R measurement is inaccurate. Measuring C is difficult, particularly if C is weak. Significant measurement for the installation. Obtaining a measurement of C is of no significance when there is an insulation fault.
Medium C, medium R The injection signal is shared between R and C. R and C can be measured correctly. Significant measurement for the installation. Significant measurement for the installation.
R and C high The injection signal that goes into R is weak. It becomes difficult to measure R and is completely impossible in the case of very high C values. C is measured correctly. Obtaining an accurate measurement of R is not important, as the system is in good condition. Significant measurement for the installation. An excessively high C value corresponds to the maximum limits of an IT system. Above 60 μF (150 μF with filtering of 160 seconds), the product is outside of its operating range and fails.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.