VIGED310022EN-06

Hardware overview

IM10 and IM20 feature 3 and 5 terminal blocks respectively (identifiers A to E).

A Injection connection terminal block
B Auxiliary power supply connection terminal block
C Insulation alarm relay terminal block
D Modbus communication terminal block ( IM20)
E Injection inhibition input terminal block ( IM20)
F Contextual menu buttons
G Operating LED
H Insulation alarm LED
I Display
J Menu button to go to the main menu
K Esc button to return to the previous menu or cancel a parameter entry
L Serial number
M Product catalog number (IMD-IM10 or IMD-IM20)

Device commercial reference

Model Commercial reference
IM10 IMD-IM10
IM20 IMD-IM20
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.