VIGED310022EN-04

Log

Applicable for IM20

The device records the details of the 30 most recent insulation fault events. The fault events are triggered by one of following statuses:

  • insulation fault

  • preventive insulation fault

Event 1 is the event that was recorded most recently and event 30 is the oldest recorded event.

The oldest event is deleted when a new event occurs (the table is not reset).

By referring to this information, the performance of the distribution system can be improved and maintenance work is facilitated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?