VIGED310022EN-04

Locating insulating fault manually

You can use the mobile insulation fault locating devices if:

  • Insulation fault location on a feeder not equipped with an automatic insulation fault locator, or

  • To facilitate the location of an insulation fault on a feeder

The signal injected by the device is not compatible with the XPxx and XRM devices. Use 2.5 Hz XGR injector.

The term “XPxx” refers to “XP15, XP50, and XP100”.

Steps:

  1. When insulation fault occurs, connect the XGR to neutral (if there isn't one, to phase) and to ground.
  2. Connect the XPxx to XRM.
  3. Clamp the XPxx and XRM setup to an inject wire near to the device.
  4. On XRM, touch and hold the ON push button, adjust the sensitivity adjustment dial and calibrate to a reference value 18.

    An example is shown as follows:

  5. Clamp the XPxx and XRM setup on all the channels and record the XRM values on each channel.

    An example is shown as follows:

    If the recorded value of a channel is nearest to the calibrated value, it indicates an insulation fault in the corresponding channel or the downstream channel (if any).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?