VIGED310022EN-04

Device features

The features supported depend on the device model.
Function IM10 IM20
Measurement and display of ungrounded system insulation resistance
Measurement and display of leakage capacitance (C)
Calculation of impedance Zc associated with C
Time-tagged insulation fault log
Communication via Modbus RS-485
Injection inhibition input
High-voltage adapter compatibility
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?