VIGED310022EN-04

Accessories

Accessories are required depending on the type of installation on which the device is installed.

Accessories list

Accessory IM10 IM20 Catalog number
Cardew C “250 V” surge limiter Yes Yes 50170
Cardew C “440 V” surge limiter Yes Yes 50171
Cardew C “660 V” surge limiter Yes * 50172
Cardew C “1000 V” surge limiter Yes * 50183
Cardew C base Yes * Yes * 50169
ZX impedance (limiting impedance) Yes Yes 50159
High voltage adaptor (IM20—1700) Yes IMD-IM20–1700

Cardew C surge limiter

Function

Cardew C is used if the insulation monitoring device is connected to the secondary connection of an MV/LV transformer (according to the rules and conventions that apply in the various countries).

It protects the low-voltage (LV) installation against over voltage hazards. It is connected to the secondary connection of the transformer. Cardew C can be used on the following systems:

  • U < 1000 V AC

  • U < 300 V DC

Selection table

Un: Nominal Phase-to-Phase Voltage of AC System

Ui: Arcing Voltage

Type of Cardew C

Accessible neutral

Not accessible neutral

U ≤ 380 V

U ≤ 220 V

400 V < Ui ≤ 750 V

250 V

380 V < U ≤ 660 V

220 V < U ≤ 380 V

700 V < Ui ≤ 1,100 V

440 V

660 V < U ≤ 1,000 V

380 V < U ≤ 660 V

1,100 V < Ui ≤ 1,600 V

660 V

1,000 V < U ≤ 1,560 V

660 V < U ≤ 1,000 V

1,600 V < Ui ≤ 2,400 V

1,000 V

Dimensions

Mounting

  • Cardew C mounted directly on busbars

  • Mounting with plate-mounted base

Connection

ZX limiting impedance

Function

ZX limiting impedance enables you to create an installation with a high-impedance grounded neutral system (1500 Ω at 50 Hz).

ZX limiting impedance can be used on the following systems:

  • Umax = 480 V AC

  • Umax = 345 V DC

Dimensions

Mounting

On mounting plate

Connection

High voltage adaptor

Function

The high voltage adaptor (IMD-IM20-1700) can be used to connect a IMD to ungrounded systems higher than 480 V AC (connection with 400 V cable).

Dimensions

Mounting

On DIN rail

Connection

(1) Voltage adaptor connected to a phase

(2) Voltage adaptor connected to neutral

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?