Safety precautions
Specific hazard associated with Insulation Monitoring Devices (IMDs)
Insulation monitoring devices are connected to the system via an injection wire, which must be disconnected before carrying out any kind of work on the product.
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION,
OR ARC FLASH
Disconnect the injection wire from the
device to the monitored system before working on the device or equipment.
Failure to follow these instructions will result in death or serious injury.
|
Other safety measures
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION,
OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Unintended Operation
Do not use this device for critical control or
protection of persons, animals, property or equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
NOTICE |
---|
Equipment damage
Failure to follow these instructions can result in equipment damage.
|