VIGED310022EN-04

Wiring diagram

All the device wiring terminals have identical wiring capabilities. The following are the list of characteristics of the cables that can be used to connect the terminals:

  • Stripped length: 7 mm (0.28 in)

  • Cable cross sectional area: 0.2 to 2.5 mm2 (24 to 14 AWG)

  • Tightening torque: 0.8 N.m (7.1 lb-in)

  • Type of screwdriver: Flat, 3 mm (0.12 in)

The illustration shows the connection of the device to a single-phase or three-phase 3- or 4-wire power system, or a DC power system.

Wiring diagram of IM10 / IM20:

NOTE: Terminals 11 to 16 are not available on IM10.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?