VIGED310022EN-04

Measurement filtering

Measurement filtering averages values over a configurable period of time.

On a system, the measurement varies continuously depending on the following:

  • Number of loads

  • Type of loads

  • Load switching

  • Size of the system (effect of C)

To prevent the display from fluctuating and to avoid inappropriate alarms, the measurements are filtered for 4 s, 40 s or 160 s.

The Filtering parameter offers a choice between the following three modes:

Filtering Description Example of use Measurement update time when monitoring the insulation Response time required to detect an insulation fault
4 s

Optimizes the response time:

  • Manual fault location phase

  • Automatic location of a transient fault

To facilitate manual location of a fault by opening each of the circuit breakers in turn 0.8 s 4 s
40 s Suitable for most applications 8 s 40 s
160 s Suitable for highly demanding applications To be used for severely disrupted power supply systems or for photovoltaic applications 32 s 160 s

The default value for the Filtering parameter is 40 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?