VIGED310022EN-04

Accuracy zone

Your device’s insulation resistance measurement accuracy varies based on the system’s capacitance as well as temperature and humidity.

Your device’s accuracy at 25°C (77°F) and 40% relative humidity.

  A Zone A: Accuracy is 20% ± 1 digit
  B Zone B: Accuracy is 5% ± 1 digit
  C Zone C: Accuracy is 50% ± 1 digit
  D Resistance at accuracy zone limit τ1
  E Resistance at accuracy zone limit τ2 (10 MΩ maximum)
     

Assuming two significant digits for insulation resistance measurements the accuracy can be calculated.

  • Zone A: At 250 Ω, 20% = 50, ± 1 digit = 10. Displayed value will range from 190 Ω to 310 Ω, for an overall accuracy of approximately ± 25%.

  • Zone B: At 1 kΩ, 5% = 50 Ω, ± 1 digit = 100. Displayed value will range from 1.8 kΩ to 1.2 kΩ, for an overall accuracy of approximately ± 20%.

  • Zone C: At 3 MΩ, 50% = 1.5 MΩ, ± 1 digit = 100 kΩ. Displayed value will range from 1.4 MΩ to 4.6 MΩ, for an overall accuracy of approximately ± 50%

Calculation of resistance for accuracy zone limitsτ1, τ2

τ = R (MΩ) x C(µF)

The accuracy of your device transitions at specific τ values, identified by testing at different resistances and capacitances, and is also influenced by the filtering (measurement sample duration) selected.

  • For filtering of 4 seconds, τ1 = 1, τ2 = 4

  • For filtering of 40 seconds or 160 seconds, τ1 = 2, τ2 = 10

Resistance at τ1 and τ2 with 4 second filtering

τ1 = 1 τ2 = 4

Capacitance = 1 µF , τ1/C = 1/1 µF = 1MΩ

Resistance at τ1 = 1 MΩ

Capacitance = 1 µF , τ2/C = 4\1 µF = 4MΩ

Resistance at τ2 = 4MΩ

Capacitance = 10 µF , τ1/C = 1/10 µF = 100 kΩ

Resistance at τ1 = 100 kΩ

Capacitance = 10 µF , τ2/C = 4/10 µF = 400 kΩ

Resistance at τ2 = 400 kΩ

Accuracy zone B (5%) range is approximately

Resistance at τ1 and τ2 with 40 second and 160 second filtering

τ1 = 2 τ2 = 10

Capacitance = 1 µF , τ1/C = 2/1 µF = 2MΩ

Resistance at τ1 = 2MΩ

Capacitance = 1 µF , τ2/C = 10\1 µF = 10 MΩ

Resistance at τ2 = 10 MΩ

Capacitance = 10 µF , τ1/C = 2/10 µF = 200 kΩ

Resistance at τ1 = 200 kΩ

Capacitance = 10 µF , τ2/C = 10/10 µF = 1 MΩ

Resistance at τ2 = 1 MΩ

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?