DOCA0216EN-00

Internal Battery (MicroLogic 6.0 B)

The internal battery powers the trip cause indication LEDs on a MicroLogic 6.0 B trip unit.

The internal battery of the MicroLogic B trip unit can be replaced on site when discharged.

Order a new battery with the Schneider Electric catalog number LV833593SP.

  • Lithium battery

  • 1.22 AA, 3.6 V, 850 mA/h

  • SAFT LS3 SONNENSCHEIN TEL-S

  • Service life 10 years

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?