DOCA0216EN-00

Testing the MicroLogic B Trip Unit

Using a dedicated test equipment, test the MicroLogic B trip unit as follows:

  1. Open the protective cover of the trip unit.
  2. Connect the test equipment via the test connector.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?