Replacement Procedure
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow these steps to change the rating plug.
- Disconnect the circuit breaker as directed in the circuit breaker instruction sheet shipped with the circuit breaker.
- Open the protective cover of the trip unit.
- Record switch settings.
- Unscrew the long-time rating plug mounting screw.
- Remove the adjustable rating plug.
- Inspect mounting area for debris and contamination.
- Take out the replacement rating plug.NOTE: Adjustable rating plug must be removed when doing dielectric testing. If adjustable rating plug is removed, the circuit breaker will default to a long-time pickup rating of 0.4 x sensor size (In) and a long-time delay of whatever setting was selected before the rating plug was removed.
- Gently push in the replacement rating plug.
- Tighten the long-time rating plug mounting screw.
- Set trip unit settings to values recorded previously or modify settings.
- Reinstall the circuit breaker front cover as directed in
the circuit breaker instruction sheet shipped with the circuit breaker.
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH- Replace circuit breaker front cover before energizing circuit breaker to help prevent access to live terminals.
- Do not pinch the wires when reinstalling the front cover.
Failure to follow these instructions will result in death or serious injury.