DOCA0216EN-00

Setting Values for Neutral Protection

The following table shows the setting values of the neutral long-time protection and pickup for the type of neutral protection selected:

Neutral protection type

Neutral long-time pickup value

OFF

No long-time protection for neutral

N/2 (factory setting)

Ir/2

N

Ir

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?