DOCA0216EN-00

Testing the Ground-Fault Protection

Test the operation of ground-fault protection as follows:

  1. Check that the circuit breaker is closed.
  2. Use a thin screwdriver to briefly push in (< 1 s) the TEST button on the front face of the MicroLogic B trip unit.
  3. The circuit breaker trips.
  4. If the circuit breaker does not trip, contact your field service representative.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?