Internal Battery Replacement
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow these steps to replace the internal battery:
- Remove the circuit breaker front cover as directed in the circuit breaker instruction sheet shipped with the circuit breaker.
- Remove the battery cover: insert a small screwdriver blade
into battery housing cover notch and rotate to slide battery housing
cover out of trip unit.
- Remove the battery.
- Insert a new battery. Make sure that the polarity is correct.
- Put the battery housing cover back in place.
- Press the Test/Reset button to
check the new battery.
- Reinstall the circuit breaker front cover as directed in
the circuit breaker instruction sheet shipped with the circuit breaker.
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH- Replace circuit breaker front cover before energizing circuit breaker to help prevent access to live terminals.
- Do not pinch the wires when reinstalling the front cover.
Failure to follow these instructions will result in death or serious injury.