DOCA0216EN-00

Trip Cause Indication LED (MicroLogic 6.0 B)

LED Description

Trip due to long-time protection

Trip due to short-time protection

Trip due to ground-fault protection

Trip due to auto-protection

NOTE: The battery maintains the trip cause indications. If there are no indications, check the battery.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?