DOCA0216EN-00

Test/Reset Button (MicroLogic 6.0 B)

Use the Test/Reset button to:

  • Reset the trip cause indications:

    1. Determine why the circuit breaker tripped. The trip cause indication is maintained until it is reset on the trip unit.

    2. Press the Test/Reset button.

    3. Check the parameter settings of the trip unit.

  • Check the battery: press the Test/Reset button to check the luminance of the trip cause indication LEDs. If the LEDs are dim, or not lit, change the battery.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?