DOCA0216EN-00

Setting the Neutral Protection

Set the type of neutral protection by using the three-position switch on four-pole MasterPact MTZ circuit breakers.

  1. Cover for neutral protection three-position switch.


Follow these steps to set the type of neutral protection.

  1. Remove the cover of the switch.

  2. Select the protection type.

  3. Put the cover back in place.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?