DOCA0216EN-00

Trip Unit Type

This code indicates the type of MicroLogic trip unit:

  • The number (for example, 6.0) defines the types of protection provided by the trip unit.

  • The letter (B) identifies the range of the trip unit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?